Other Parts Discussed in Thread: PMP
My board uses the TI_AM572x_PM_RevA3a reference design except with the newer PMIC part number TPS6590378. From what I've read, this PMIC is pin-to-pin compatible with TPS6590376, so I'm not expecting the change to -8 to be the cause of my issue. I measured the voltage rails and they are as expected; however, PMIC_POWERGOOD (pin J7) is low.
My best guess is that this is a side effect of using pin G9 (GPIO_7) as POWERHOLD. On my board, Pin G9 is connected to LDO_VRTC through a 10K resistor in order to power on without a power switch. From the PMIC datasheet I found that GPIO_7 can also be used to monitor an external SMPS. Could using GPIO_7 for POWERHOLD rather than monitoring be why the PMIC power is not good?
Also from the PMIC datasheet I found that all POWERGOOD sources can be masked in SMPS_POWERGOOD_MASK1 and SMPS_POWERGOOD_MASK2 registers. Is this is a reasonable fix to get POWERGOOD to indicate power is good? If so, where can I find instructions to change the registers?