Hello Team,
Is it possible to set the current value of each channel as follows?
And, is it possible to realize if the thermal design can be cleared?
Is output of 5-6A difficult to realize without connecting output 2 channels?
OUT1:Iout_max = 5-6A
OUT2:Iout_max = 1A
OUT3:Iout_max = 0.5-1A
OUT4:Iout_max = 0.5-1A
Best regards,
Kato