Other Parts Discussed in Thread: TPS653850-Q1
Hello PMIC team,
I have 2 questions about TPS65381A-Q1
Q1. When current-limit condition is no longer present, does the “VDD5_ILIM” register automatically change to “0”? Or will it be latched to “1” until the MCU read this register?
D[7] VDD5_ILIM: VDD5 current-limit status bit
– Set to 1 when a VDD5 current-limit condition is exceeded
– Cleared to 0 if a current-limit condition is no longer present
Note: This status bit is valid only when the VDD5_EN bit in SENS_CTRL register is set to 1. When the VDD5_EN bit is
cleared to 0, this bit will be 1.
Q2. When overvoltage condition is no longer present, does the “VDD5_OV” register automatically change to “0”? Or will it be latched to “1” until the MCU read this register?
D[5] VDD5_OV: VDD5 overvoltage status bit
– Set to 1 when a VDD5 overvoltage condition is detected
– Cleared to 0 if an overvoltage condition is no longer present
Let me know if you have any question,
Thanks,
Yuta Kurimoto