A related question is a question created from another question. When the related question is created, it will be automatically linked to the original question.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
[FAQ] TPS650830: What's the special need for TPS65083x VIN3 and VIN5 Connections?
Note that it is critical to connect the VIN3/5 to the VIN for the FETs of the respective controller. The VIN3 and VIN5 are used as sense lines to the VIN of the FETs in-order for the high side current limit to work properly. Therefore, be sure to connect them as close as possible to the High Side FET's VIN pad.