Q: While using digital mic inputs on TPS65950, is there any specific procedure to enable digital mic clock?
A: No. However, you can use the same procedure mentioned in the TRM and have the digital microphone enabled at the same location where you have analog microphones enabled.
Q: How to setup the clock speed?
A: CLK speed is set by the APLL_RATE (50*FS). In this case you have only 48K as mentioned in TRM.
Q: Will the digital mic clockout depend system clock(13M, 19.2M or 26M)?
A: Any system CLK is fine.
Q: Will this digital mic clock present always? Or only present when enable?
A: Digital microphone interface is enabled only when you set it in PMBR1 register. So, CLK is not present always.