Hi,
the TRM shows that for the row inputs on the keypad interface there are internal pullup resistors. If one were to use additional external pull-ups, which voltage should they be pulled to?
Thanks,
--Gunter
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
additionally the Mistral DM37xx EVM is using external 4.7K resistors pulling to VIO_1v8. There is a note in the TRM that if a smaller keypad area is used, the unused row/column inputs are recommended to be pulled up. Should a good design use external pullups to be safe from false scanning? And secondly what voltage should the pins be pulled to? It is not clear from the TRM/datasheet.
Thanks,
--Gunter
Hi,
the feedback was that there are internal PU resistors and external are not needed. My followup question is that in the TPS65950 datasheet there is the following line on page 130:
"The keyboard interface can be used with a smaller keyboard area than 8 × 8. To use a 6 × 6 keyboard, KBR(6) and KBR(7) must be tied high to prevent any scanning process distribution." So that raises the question again, whether external PU resistors could be needed. Could someone clarify? Thanks, --Gunter
External resistors are not needed. I will have to fix the document. I believe the document was providing a very conservative approach to avoid false scanning as you have pointed out.