What is the absolute maximum voltage limit (positive and negative) for adc (2 - 7) of TSP65950?
I could not find in datasheet. It only provides full scale voltage range.
Thank you.
Sudil,
Table 3.1 page 27 show that absolte maximum voltage are 0V and supply voltage.
Supply voltage is defined for each pin in table 2.1 page 16. Please look at the Reference level column.
For ADCIN2 to 7, it's VINTANA2 which is 2.75V
http://www.ti.com/lit/gpn/tps65950
regards,
Alexis
------------------------------------------------------------------------------------------------------Kindly click the Verify Answer button on this post, if it answers your question.------------------------------------------------------------------------------------------------------