Hi,
I am facing some issue in our customzed boards design where we use AM3359 Silicon Rev 2.1 with TPS65910AA1RSL. I have also discussed the following issue with TI rep on the same subject in Sitara forum. I am posting it again here.
VDDS_RTC of AM3359 is getting powered from VRTC(pin29)of PMIC. The board was working fine few days but suddenly PMIC became non functioning. I took the measurement on that pin it is about 1.4V instead of 1.8V. AM3359 is unable to provide PMIC_Power_Enable signal to PMIC.
When I gave 1.8V externally to that pin, It is back to working. So I have following queries:
1. what is the best to solve this problem? I am also aware that external LDO is suggested.
2.How it should be done? do we have to short external LDO output and VRTC output of PMIC together?
please help me clear this doubts.
Regards,
Ibram