Hello.
This is more of a general question concerning the operation of the USB OTG. Can you provide more specifics on the internal operation of the PMIC's internal USB circuitry? For example, how does PMIC resolve collisions between the CP voltage and the voltage on VBUS supplied by the remote host? What should be done to route the CP voltage to the VBUS pin of the PMIC? Can this voltage be used to supply a 5.0V level for various purposes (i.e., setting the rail for I2C communications with an IC whose logic is powered with 5.0)?
Thank you in advance