Hi,
We're using a DM3730 based design similar to beagle-xm. We're having a small percentage of units fail in production. In this case, the mode of failure is that the unit fails to boot, and the D12 LED (PMU_STAT / LEDB) which is driven by the TPS65950 fails to get asserted. This does not involve any system software as the NAND flash and microsd interfaces are empty. The boards that fail in this way do not have the LEDB signal asserted. The good boards (also empty flash, microsd) get LEDB asserted. My understanding is that this signal is driven by BootROM. I have not been able to find out what would be the cause of failure / error detected by BootROM that would cause it to fail to assert LEDB. Am a bit stumped and looking for any ideas/suggestions. I've checked the sys_boot strappings and the failing boards have the same values as the good boards.
Thanks,
jayakumar