Using TPS65910A1RSL for OMAPL138 with boot mode pins on TPS65910A1RSL connected as BOOT0=GND, BOOT1=VRTC (recommended by the"TPS65910 User Guide For OMAPL-137, OMAPL-138, and TMS320C674x Family of Processors")
Can the internal RC oscillator be used or do I have to connect external crystal or oscillator? The datasheet for TPS65910A1RSL indicates the internal oscillator usage is dependent on the BOOT pin configuration.
The document says:
The device supports three embedded power sequences selectable by the device BOOT pins.
BOOT0 BOOT1 Processor Supported
0 0 AM3517, AM3505
1 0 OMAP3 Family, AM3715/03, DM3730/25
0 1 EEPROM sequence
The document also states:
Default selection of a 32-kHz RC oscillator versus 32-kHz crystal oscillator or external square-wave 32- kHz clock depends on the Boot mode or device version (EEPROM programming): •
BOOT1 = 0, BOOT0 = 1: quartz oscillator or external square wave 32-kHz clock default •
BOOT1 = 0, BOOT0 = 0: 32-kHz RC oscillator default
This addresses two (0,1 and 0,0) but does not address the recommended BOOT1=1 and BOOT0=0 (1,0).
What is the behavior when BOOT1=1 and BOOT0=0?
Does Table 4 in TPS65910 User Guide For OMAPL-137, OMAPL-138, and TMS320C674x Family of Processors imply RC OSC is not an option (CK32K_CTRL as 1=RC_OSC)? (I thought I saw somewhere where these were factory set. "The correct power-up sequence is configured in the EEPROM (factory programmable only).")
DEVCTRL_REG RTC_PWDN 0 = RTC in normal power mode 1
1 = Clock gating of RTC register and logic, low-power mode
DEVCTRL_REG CK32K_CTRL 0 = Clock source is crystal/external clock. Crystal
1 = Clock source is internal RC oscillator