How to read VBUS voltage from MADC in TPS65930/20? Is it the same as TPS65950 including the enable bit for the prescaler? Is MESVBUS within BCICTL1? The BCICTL1 description is not found within TPS65930/20 document.
THanks,
Antony
Hi Antony,
Yes, you are right. Please use the same method as mentioned in TPS65950. When the BCI chapter was deleted for TPS65930/20, the BCICTL register info was also removed. I will get this information added in the MADC chapter.
Regards,
Gandhar.
Regards,Gandhar------------------------------------------------------------------------------------------------------Kindly click the Verify Answer button on this post, if it answers your question.------------------------------------------------------------------------------------------------------