Q : What features do the TPS65930 and TPS65920 devices offer
compared to the TPS65950 ?
A : The TPS65930 and TPS65920 offer a subset of the features
available from the TPS65950 :
Both the TPS65930 and TPS65920 (compared to the TPS65950)
- No battery charger capability
- No DC vibrator drive capability
- Two switching supplies available
for external loads (instead of three)
- Three low-dropout linear regulators
for external loads (instead of seven)
- Two external GPIO inputs (instead of eight)
- A 6x6 keypad interface (instead of 8x8)
- No MCPC functionality in the USB section
The TPS65930 (compared to the TPS65950)
- Reduced audio functionality including
no PCM and no Bluetooth interface
The TPS65920 (compared to the TPS65950)
- No audio features (this includes
no analog vibrator capability)
The TPS65930 and TPS65920 (compared to the TPS65950) are in
packages which have fewer pins and increased spacing between
the pins.