• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Power Management » PMU » TPS659xx PMU Forum » All Tags » RTC
Share
PMU
  • Forums
  • Announcements
  • E2E Wiki

Browse by Tags

PMU

Welcome to the PMU Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Sign In to Post
Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
RTC
  • alarm interrupt
  • am335x
  • back up
  • backup
  • back-up
  • backup battery
  • backup mode
  • BKBAT
  • compensation
  • current
  • mistral
  • Mistral board
  • TPS65023
  • TPS65910
  • TPS65910A
  • TPS65910A3
  • TPS65910A31
  • TPS65910Ax
  • TPS6591X
  • TPS65920
  • TPS65921
  • TPS65950
  • TPS659xx
  • TWL4030
  • VBACKUP
Related Posts
  • Forum Post: TPS65950/30/20: RTC current

    Gandhar Dighe Gandhar Dighe
    Q: What is current consumption/specification for running the RTC only. A: RTC is supposed to supply only the backup domain and in backup mode this consumption is 2.25uA. This is the value when 32k is in low power mode and device in OFF state.
    on Feb 18, 2009
  • Forum Post: Still Confused By Documentation Discrepancies - TPS65920 RTC - Held Up Awaiting Answer

    Howard Robson Howard Robson
    I posed this follow on question on 3/30/09 in a previous post and am still awaiting and answer. The design is held up awaiting clarification on the question this further documentation discrepancy I am trying to find the current drain of th RTC to determine battery life. The only reference I can find...
    on Apr 6, 2009
  • Forum Post: TPS65950/30/20: Backup battery

    Gandhar Dighe Gandhar Dighe
    Customer question: Q: Can we consider that connecting a back-up battery will keep the PMIC RTC powered even if the main battery is unconnected? A: Yes, please refer to the state diagram in the Resets and Power Management chapter in the TRM.
    on Apr 30, 2009
  • Forum Post: Accessing RTC registers

    Antony Lin Antony Lin
    I tried to access RTC register but found I failed to change the TC register values. In addition, RTC is not running (all TC registers are '0'.) MSECURE is high on my board. I also set STOP_RTC='1', and check RUN='1', too. Did I miss anything? Thanks, Antony
    on Jul 28, 2009
  • Forum Post: Re: Accessing RTC registers

    Antony Lin Antony Lin
    Hi Kartik, Thanks, it works now. I didn't set get_time.
    on Jul 28, 2009
  • Forum Post: Re: TPS65930 RTC

    Gandhar Dighe Gandhar Dighe
    Hi Rejo, You can refer to the document pointed by Mike. This document explains how 32K clk can be compensated and adjusted using TPS65930 registers. It is possible to adjust accuracy to 1/32768 seconds per hour. However, the external porocessor needs to calculate the value to be programmed in the...
    on Aug 13, 2009
  • Forum Post: Re: Linux driver for TPS65930 RTC

    Gandhar Dighe Gandhar Dighe
    Hi Subash, The RTC does not work with Mistral hardware because MSECURE is not pulled high. MSECURE needs to be pulled up for RTC to work. If you need secure operation then you also need to connect MSECURE from TPS659xx to OMAP DRM_SECURE pin. Both these fixes will need hardware modifictions on the...
    on Aug 18, 2009
  • Forum Post: TWL4030 Compensation techniques

    Gandharva Kumar Gandharva Kumar
    My customer has the following doubt; does anybody know of any other technique to compensate the RTC of TWL4030. The purpose of this mail is to explore the techniques available for compensation of drift in RTC Timing. The conventional approach suggested in http://focus.ti.com/lit/an/swca024/swca024...
    on Oct 12, 2009
  • Forum Post: Re: TPS65930 RTC Time register Access issue

    Gandhar Dighe Gandhar Dighe
    Hi Rejo, Do you set GET_TIME bit every time you try to access the calendar registers? Please refer to thi spost also - http://e2e.ti.com/forums/p/6586/25405.aspx#25405 Regards, Gandhar.
    on Nov 2, 2009
  • Forum Post: Re: TPS65950 - RTC wake up on predefined counter / alarm

    Gandhar Dighe Gandhar Dighe
    Hi Keith, We dont have a document for this. However, here are some steps that customer can follow: Set the time in the RTC time registers - year, month, ....., seconds. Make sure MSECURE is HIGH for this operation. Then, you can set the RTC alarm registers for any specific time, set IT_ALARM='1'...
    on Nov 19, 2009
  • Forum Post: TPS65950 RTC Current

    Graham Woods Graham Woods
    Hi, Can you tell me what the current consumption is for using the RTC function on the TPS65950 please. Ive looked through the datasheet but I cannot seem to find this information. Thanks Graham
    on Mar 22, 2010
  • Forum Post: Re: RTC does not keep time after 2 days on the tPS65930?

    Gandhar Dighe Gandhar Dighe
    Hi Mohsen, Can the customer check or be very sure that backup voltage is at 1.88V at all times. If there is a glitch for a short period when the battery is off then the RTC will have no power and data will be lost. Regards, Gandhar.
    on Jun 24, 2010
  • Forum Post: Re: can a capacitor instead of battery be used on pin VBACKUP for backup purpose?

    Jiansheng Liu Jiansheng Liu
    Thanks for the reply. I checked the datasheet that describes a capacitor in a range of 5 to 2000mF, that is huge! Are we sure it is not a typo of 5 to 2000uF?
    on Nov 10, 2010
  • Forum Post: TPS65950 RTC Battery Backup - Configuration required?

    Josh Watts Josh Watts
    Does the battery backup feature of the TPS65950 require any configuration or setup? Or should it work perfectly well "out of the box"? In our design, we have BKBAT connected to a small lithium coin-cell battery, currently charged at 3.0V. Both sudden loss of power and proper shutdown of...
    on Feb 8, 2011
  • Forum Post: Re: TPS65921 RTC battery backup capability

    Jeff Mogensen Jeff Mogensen
    Alexis, That is interesting since I am able to keep the RTC alive using a 3V coin battery connected to the TPS65921 BKBAT when the main battery has been removed from VBAT. The main battery has been removed for a over a week and time has been maintained. Perhaps VRTC is being supplied via the BKBAT...
    on Apr 13, 2012
  • Forum Post: TPS65921 RTC battery backup capability

    Jeff Mogensen Jeff Mogensen
    I have connected a battery to ball G9 BKBAT VBACKUP and have maintained the RTC after removing power main power VBAT. The documentation on the TPS65921 states that ball G9 BKBAT VBACKUP must be shorted to GND, yet the documenation also states the VRTC.OUT output voltage range for both "Normal...
    on Apr 5, 2012
  • Forum Post: TPS65023 and Backup Coin Cell Battery

    Saad Habayeb Saad Habayeb
    Hi, I'm using a coin cell battery with the TPS65023 for a real-time chip. the main power to the board is 5V through a AC-DC supply (not a portable device). The microprocessor is a TI AM3505. The problem is that on cold power-up the micro does not start correctly until the reset button (connected...
    on Oct 3, 2012
  • Forum Post: tps6591x rtc WEC7 OALIoCtlHalInitRTC problem

    Thomas Coin Thomas Coin
    Hello everyone, I'm trying to use the external RTC on the AM335x EVM (WEC 7), using the TPS6591x, but I've got some troubles initializing it. What does have to be done in the OALIoCtlHalInitRTC function ? How to check at init if the RTC has been rested or if it's running normally ? Regards...
    on Jan 3, 2013
  • Forum Post: can a capacitor instead of battery be used on pin VBACKUP for backup purpose?

    Jiansheng Liu Jiansheng Liu
    I wonder if it is possible to use a capacitor instead of battery connecting to pin TPS65910's VBACKUP for temperary backup purpose? I don't expect it is able to last for ever, but just for a few of minutes. Is it possible? If it is how big a capacitor be considered? There is a capacitor in range...
    on Nov 9, 2010
  • Forum Post: RE: TPS65910Ax Built-in RTC

    Frank O Frank O
    Hi, Any updates on this topic since November 2012? As I also consider using the TPS65910A3 RTC with a battery on VBACKUP pin. According to another thread on this forum, the EEPROM Bits are reloaded from a OFF to Active state transition. (http://e2e.ti.com/support/power_management/pmu/f/43/t/225987...
    on Jun 11, 2013
  • Forum Post: TPS65910Ax Built-in RTC

    Daisuke Maeda Daisuke Maeda
    Our customer want to use TPS65910Ax Built-in RTC. RTC is configured by EEPROM Configuration as follows. - Clock gating of RTC register and logic, low-power mode - Clock source is internal RC oscillator TPS65910Ax User's Guide For AM335x Processors (Rev. B) http://www.ti.com/lit/ug/swcu093b...
    on Nov 1, 2012
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use