Q: TPS65735/TPS65835 Boost Start-Up Issue by 1129650

The boost converter on my TPS65835 (or TPS65735) EVM does not tun-on to the full output voltage of 10V.
The output only powers up to about 8 volts; why is this?


A: Re: TPS65735/TPS65835 Boost Start-Up Issue by 1129650

The TPS65735 and TPS65835 boost converter cannot start up into a full load. Remove the load, cycle power then load after the boost output is in regulation.