Welcome to the PMU Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".
Q:
From datasheet I think /INT goes Low at following condition. Is my understanding correct?- Supply correct VCC voltage (ex. 3.3V or 4.2V)- HOTRESET = High- DCDCx_EN and LDO_EN = High- one of VDCDCx or VLDOx goes down to around 90% of required output level
Could you let me know what status /INT will be when all of DCDCx_EN and LDO_EN are Low (while any PGOODZ<n> is unmasked) ?
A: The /INT output will go low as following - /INT will remain low during power up, once all enabled rails are within regulation /INT will go high impedance - whenever any of the enabled rails falls out of regulation /INT will go low - when the PGOODZ register is read via I2C /INT will go high again even if the rails is still not within regulation. HOTRESET or VCC or EN_DCDC/ EN_LDO pins of the device do not have a direct impact on the /INT output In your described case, /INT should be high impedance
A:
The /INT output will go low as following
- /INT will remain low during power up, once all enabled rails are within regulation /INT will go high impedance
- whenever any of the enabled rails falls out of regulation /INT will go low
- when the PGOODZ register is read via I2C /INT will go high again even if the rails is still not within regulation.
HOTRESET or VCC or EN_DCDC/ EN_LDO pins of the device do not have a direct impact on the /INT output