Welcome to the PMU Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".
Q: TPS65023 VRTC by 1116450
Does the TPS65023 need a capacitor on VRTC (pin 16) if VRTC is not used (floating)?
A: Re: TPS65023 VRTC by 1129650
Yes, the capacitor is needed on VRTC even if it is unused. VRTC may oscillate if the capacitor is not present.
Also note, VRTC is an input to the comparator for /RESPWRON.