I am going to connect and LM5066 to an AM3359 I2C bus 2. I am not sure if I am supposed to connect the SDAI and SDAO lines together. There is a forum post on here relating to the LM5064 that says to use an ISO1540 to separate them, but the dev kit and the datasheet for the LM5066 show the lines as directly connected. There is nothing else on I2C bus 2.
Is there a particular pin on the AM3359 (ZCZ) that I should use for the SMB Alert! signal, like a 'driver default' pin?