Question/Problem:
If both IN1 and IN2 are not present, can D0/D1 be connected to 3.3V?
Answer:
Yes, an internal blocking diode with the Anode connected to the internal VDD rail and the Cathode connected to the control logic input prevents these inputs from biasing the device.
Thanks,
Leslie C.