Power Interface
Forum
E2E Wiki
Options
Subscribe via RSS
TPS2111 - Can I set Rlim=0ohm?
TPS2111 - Can I set Rlim=0ohm?
This question is not answered
Posted by
Leslie Chataway
on
Aug 25 2008 09:25 AM
Mastermind
20970
points
Question/Problem:
Can I set Rlim=0ohm?
Answer:
Yes, but this can cause excessive power dissipation and damage to the device. If you are certain that the power dissipation is not a problem, then setting Rlim to zero is acceptable.
Thanks,
Leslie C.
Rlim
TPS2111
Report Abuse
Reply
You have posted to a forum that requires a moderator to approve posts before they are publicly available.