Hi all!
There is a current limiting circuitry using TPS24710DGS in the attachment file.
Requirements are:
Voltage: 10.8V to 13.2V
Ilim Current: 50 mA, Rsense = 510 mOhm.
However real current limit is 25..30 mA, not 45-50 mA.
The calculated value of TPS24710 current limit doesn't coincide with the real value.
Anyone can please review this design and explain, why?
Thanks in advance.
Best Regards,
Svyatoslav.