Hi, I'm trying to use the pspice model for the tsp25944l, but it seems to be broken. When the simulation is enabled into a prebiased Vout - as it could be used in actual application, the output is grounded and then ramped up according to dVdT. I don't believe that that is the intended functionality, nor physically possible looking at the datasheet.
Also defying physics is the fact that no current enters the IN side of the device, although it does exit the OUT pins. So in effect the part is acting as an energy source. I test by taking the example circuit, and adding a 1mohm resistor on the input side, and measuring input & output current. Attached is a screen shot of the simulation output.
Can I get an updated model with these issues fixed please?