This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Hong,
We cannot support this question in the load switch forum, however it can be answered in the power interface forum which is where we are moving your question. Load switches have a maximum input voltage of 5V, and can only support up to 15A. Power Interface does have higher voltage and current devices similar to the max14653.
Thank you,
Adam