I have put together a POE PD design based on the 12W LM5072 reference design and a custom transformer which would allow for a 24v secondary which I regulate on. The basic functionality works, but the MOSFET SUD15N15 overheats on a very basic load of 100ma let alone the 500ma which I need it to operate it at. Just looking for some suggestions on how to attack this, I know I must have something set up wrong, and was considering moving to the 25W design. I am including the gate-source and source-drain waveforms for reference. The gate source is at 5v/div .05us/div, the drain-source is 50v/div .05us/div.