Hi, I'm Byoungkil Jung from Korea.
I'm sorry because I have a poor english ability.
I have a plan to use Hot-swap controller, TPS24700 or TPS24701.
But I have some questions about this ICs.
TPS24700 is Latch off type and TPS24701 is Auto retry type.
As seeing the Fig28 & 29, at the overload condition, two types are operating differntly..
but I didn't understand exactly between two types.
I have been understand as follows;
Using the TPS24700,
at the overload condition Timer starts.
and after ending overload condition, TPS24700 IC turns on?
Using the TPS24701,
at the overload condition Timer starts.
and after 16 Timer cycles, if PGb is low, TPS24701 IC turns on?
Plese explain the Operation of two types at the overload condition.