For LM5060 over current setting, it is depended on following 2 equations, and Voffset is one of variations. I check the Voffset value which is between -7mV to 7mV.
I check demo board’s setting, and 5.8A is the typical over current setting. Rs is 9.09kohm, and Rds is 25mohm. Based on those value and equation, Voffset is around 0.00044. Actually, I have not question on this value, but I want to know how to define this value? Thanks.