Dear Sir
TPS2592 current limit show type is 5A ,
If I set Rlim to 175kohm ,is the current limit still keep 5A or will be changed to 6A?
What's the situation I will meet?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Operating continuously above 5A is not recommended and the maximim recommended Rilim is 162kohm. Using 175kohm will yield a higher Iscl and potentially a continuous Iout higher than 5A depending on your load.