Dear specialist
Our customer is considering to reduce leak current.
Could you please support their questions as below?
Q1.
Condtion
- Power unit is in sleep mode
- IN,VS,OFF pin is 0V
- Only OUT pin is applied from 6V to 16V.
In the above case , Are there any issues ?
In the above case , Are there any issues ?
Since they measured leak current that is 0A at OUT pin , If no issue , they will apply the above condition.
Q2.
When power supply of VS pin is applied from OUT pin (LOAD side) , is it OK that between LOAD and OUT pin is placed about 10kohm?
Best regards.