In the datasheet, it shows the power limit.
May I know the definition of power limit, I2xRON or others?
Power limit VIN: 12 V, COUT = 1000 μF, EN: 3 V → 0 V 3 5 7.5 W
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
In the datasheet, it shows the power limit.
May I know the definition of power limit, I2xRON or others?
Power limit VIN: 12 V, COUT = 1000 μF, EN: 3 V → 0 V 3 5 7.5 W
Hi James,
The TPS25910 falls under the Power Interface group. I will go ahead and move this thread to their forum.
Regards,
Alek Kaknevicius
Hello James,
You got is right...
The power limit in the data sheet is the power dissipation limit on the FET for this to be in SOA.
This is defined by following ways-
Id x Rds = Vds x Ids =Vds^2/Rds
Regards
Dinesh