hi my customer B is asking about the operating ratings on page 3 of the datasheet.
They mentions up to 85 Deg TJ but the part has a TJ of 150DEGREE.
is there a typo?
REGARDS,
KAMAL
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi my customer B is asking about the operating ratings on page 3 of the datasheet.
They mentions up to 85 Deg TJ but the part has a TJ of 150DEGREE.
is there a typo?
REGARDS,
KAMAL
Hi Kamal,
Note that the original National datasheet had the same 85C information:
We are digging into this to see if this is a typo. Because it is a formerly National device, it will take some time to find and analyze the original char data.
The datasheet includes curves of several parameters up to 125C (Figures 10-20). These curves indicate typical values which look ok and would not affect the device's ability to operate at that temperature. But because they are typical values, we must find the char data to see if the EC table values are taken at 85C or 125C.
Thanks!
Alex
Hi Brian,
my customer needs support for 125C. As I understand, the LM25069 can support 125C because the characterization was actually done at 127C.
Even though the datasheet says "Operating Ratings Junction Temp. Range: -40C to +85C", it should actually say -40C to +125C.
Can you confirm my understanding is correct?
As the FET is external I would inform my customer that they need to check if it supports 125C.
Do you have any other concerns besides the FET?
Thanks! Appreciate your support!