HI,
Could any one help for this question?
We has tested the reverse-voltage protection function last week, and found out that:
- When they power on the 2553 first(Vin=5.1V) and put a voltage(5.5V) form another power supply which is 135mV higher than Vin on the Vout, the reverse-voltage protection don’t work and the fault pin keep to be high. This seems not right for them, they hope us could explain it for them.
- When they put the 5.5V on Vout first and power up the 2553 with 5.1V(Vin), the reverse-voltage protection function works well, and the fault pin turn be low. This seems right for them.
Does any one know whether this is normal? And why?