Dear all.
We are using two LM5050-1 to or two different supplies.
The VS-pin is connected to the out pin via a 100Ohm.
When i disconnect one of the inputs, i can still measure a voltage of about half the voltage on the other input(ored output).
Is this a correct behaviour of the chip or is there anything wrong?
This is a problem for me because I want to measure the input voltage on both inputs with a >300kOhm resistor divider. And for me this behaviour looks like there is an supply conntected.
Best regards,
Robert Steinbauer