We've developed some boards using TPS2592ZA and considering the datasheet SLVSC11B. This document says that recommended continuous output current is from 0A to 5A and the R_ILIM recommended range is from 40.2k to 162k.
This week I found out that a new datasheet was released, SLVSCU3. The parameters mentioned above were changed in this document: recommended continuous output current now is from 0A to 1.7A and R_ILIM recommended range now is from 10k to 45.3k. As it's a substantial change, I'm worried about our design, even though we've performed a lot of tests.
Some of our loads have high and large current peaks during their initialization (8A x 30ms and 5A x 100ms), but average/continuous current is less than 1.6A. Due to these peaks, we've to select a R_ILIM of 150k, which corresponds to I_OL of 5.2A and I_FASTTRIP of 8.3A.
Regarding the new limits of new datasheet, our average current is ok, but R_ILIM is above the recommended range. Resulting voltage at ILIM pin with 150k is 1.5V, well below the ILIM open resistor detect threshold (3.1V).
My question is: It's ok to use a 150k resistor at TPS2592ZA ILIM pin in order to accommodate the mentioned peaks since continuous current is within the recommended limit?
Need any additional information to evaluate this question?
Thanks