Hello TI,
I have a customer starting a new design. He needs POE PSE capability.
We're looking at the TPS23861 and have some questions:
1: Can this device support passive POE?
2: If it can support passive POE can it do it at 24 or 48V?
3: Can I test the demo board in passive POE?
Thought is it can be done if we put the device in control and monitor mode. In this mode all controls are under micro controller!
I look forward to your answers.
Dan