Hi,
We have a custom design using TPS23751 to implement 5V poe output. Attachment is the schematic. Almost same as TPS23751-EVM except some MOSFET.
For light load VFO mode, 5V output is fine. But we meet with 2 questions for PWM mode.
1: When the load is medium, for example 3ohm-3.5ohm, the SRD output waveform switch from 0 - 12V periodically, it's not stable 0 or stable 12V. We can force it work in PWM mode by setting SRT to zero, but we get the following second issue.
2: The output can't get 5V in PWM mode, only 4.6V for medium load, as the load increase, the output voltage goes up. It can get 4.9V when load is 4A. The pin1 of TLV431 can't fix in 1.25V, it only has 1V. It seems the total TLV431 feedback system can work normally.
Please advise how to debug this issue, thanks!