TPS2490 does not latch off when a fault occurs. It does a restart after the fault is removed. I was using a TPS2491 initially, but wanted to change to TPS2490 to latch off when a fault occurs. The TPS2490 seems to act the same as the TPS2491. Why does it not latch off when a fault occurs?
The schematic is the same as the EVAL board schematic except the EN pin has resistors (240K & 15K) that set it for 24 VDC operation rather than 48 VDC operation. The voltage on the TIMER pin (Pin 4) reaches 4 V after approximately 17 mS at which time the gate voltage should drop to 0 V and it should latch off. The gate voltage does not drop to 0 V and it does not latch off.