Hello,
We are using the TPS2553 current limiter in our circuit.
During our tests we have discovered a strange behaviour.
While waking up the TPS2553 to Vin = 6.5V, with no load on output and EN is tied low, it seems that the input current rises up to ~20uA for the first about half a second and then falls to less then 1uA (As indicated in the data sheet) after about 4 sec...
This phenomenon gets worse as we lower the temperature, we've had pulses of over 1uA for as long as 2 seconds at around -30deg celsius.
Do you have any explanation for this behaviour?
Thanks,
Waiting for your reply,
Eli.