In page 31 in the TPS2546, there is an equation that gives the i_lim resistor value, which would correspond to a certain output current limit. Using this equation: If I want my current limit to be 1.50 A, I should use: 50,250/1.5 A = 33.5 kOhms. However, on page 29 in the example application (figure 38 .. with 2 TPS2546 chips), there is a resistor of 29.8 kOhms to set a current limit of 1.5 A.
So, 33.5 kOhms vs. 29.8 kOhms. There seems to be an inconsistency here.
Basically, I want to know what resistances correspond to the following current limits: 0.9A, 1.0A, 1.5A, 2.0A, 3.0A.
Thanks,
Matt