Hi,
I would like to know if TPS23756 can meet our product design specification.
Our design specification as below,
1. PoE PD 802.3at class4.
2. Input voltage DC 42.5 V~57V by RJ45 cable.
3. Output : 13V / 1.9A
Should I use Flyback or Forward topology ?
I have EVM of TPS23754 (TPS23754EVM-420/HPA420 REV.B) here,
but I would like to test TPS23756 ,can I replace with TPS23756 IC and don't change
the other components on TPS23754EVM-420?
Thank you for your help!