Hi,
Could you tell me about TPS25910.
Customer is going to use the TPS25910 under the following conditions.
・Input Voltage : 17V
・Cext : 0.1nF
・Rlim : 30kΩ (Ilim≒6.5A)
・Cout : 330uF
Can I use an TPS25910 in this condition?
Please tell me if there is a concern.
This device does not correspond to the simulation.
Therefore, Customer is troubled with a judgment.
Best Regards,
Yusuke / Japan Disty