Hi,
I would like to know the impedance between the GND pin and the other pins, nPGD,UVLO,OVP,EN, etc.
Please tell me the information if there is.
It is necessary for us to check the current pass at reverse battery condition.
Best regards.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I would like to know the impedance between the GND pin and the other pins, nPGD,UVLO,OVP,EN, etc.
Please tell me the information if there is.
It is necessary for us to check the current pass at reverse battery condition.
Best regards.
Hi Alex,
Thank you for your reply.
We had designed in reference to figure 38.
Also it is insertion resistance for the current limit at the time of reverse connection.
I am concerned that there is current pass to EN pin or nGND from GND pin through the inner diode or test circuit.
EN pin and nGND pin are connected to interface and VDD of microcomputer.
Is there the situation like that?
Best regards,
Tomoaki Yoshida
Hi Alex,
Thank you for your reply.
I understood that current leak path to EN pin from MCU's FET body diode.
I will check that the MCU is open-drain or push-pull.
Can you think other current leak path from other pins in using like figure.38?
Best regards,
Tomoaki Yoshida
Hi Yoshida,
No I do not see other leakage paths.
A couple of months ago, I captured waveforms of testing the Figure 38 circuit. See the PPT attached:
LM5060 Reverse Polarity Protection.pdf
Thanks!
Alex
Hi Alex,
If the microcontroller has body diode, how much the leak current will be supposed?
Vbat will be -12.5V at reverse polarity.
I would like to estimate the delay time from Enable is turned high to the Gate will be over Vth.
Simply, Can I calculate the time is charge the parasitic capacitor of gate by Igate?
We're worried about other factors are involved.
Best regards,
Tomoaki Yoshida
Hi Yoshida-san,
The LM5060's EN delay is not spec'd in the datasheet, but it should be on the order of microseconds. After this brief delay, the time it takes to charge up to the 5V Vgs-th (the point where the IC resets the TIMER during startup) would be as you mentioned, the parasitic capacitance of the MOSFET's GATE being charged by a 24uA typical constant current source (charge pump). Overall, we suggest sizing the timer to be at least 2-3x the typical startup time, due to variance in the gate charging current, the Vgate-th value, mosfet capacitance and timer thresholds. To get a rough estimate of the typical startup time, you can look at the MOSFET's charge curve to see what value it would take to get to 5V Vgs. Most MOSFETs will be around 30-100nC which would take ~1.25ms - 4ms (since I = coulombs/second --> 24uA = 24uC/s = 24nC/ms). If the design uses parallel MOSFETs, then this time would increase.
Edit: As for the EN current through the microcontrollers body diode in a reverse polarity condition, that would only occur if the microcontroller is also seeing -12.5V and there is a pull-up resistor from Vin to EN. If so, then its open drain FET's body diode would conduct, and the leakage current would be roughly Vin / Ren where Ren is the pull up resistor used from Vin to EN for the LM5060 design.
Thanks!
Alex
Hi Alex,
I would like to check the pull-up resistor between Vin and EN that you said.
I understood the pull-up resistor means external and there is not internal pull-up resistor.
Is it correct?
Best regards,
Tomoaki
Hi Alex,
Thank you for your reply.
I would like to know Vgs at low Vin condition.
For example, when Vin is 5.5V, how much is lowest Vgs?
If the efficiency of the charge pump is 90%, Vgs is 9.9V.
However , if it is 80%, Vgs is 8.8V.
Also, at low Vin case like that, is there a problem of heat of IC to fell the efficiency of the charge pump?
Best regards,
Tomoaki
Hi Tomoaki,
We are digging into this.
First we are checking if this is tested within our final test program (Vgate at min Vin, 5.5V).
To give some insight into this device's charge pump, it is a 3-stage charge pump. The internal regulator voltage is about 5V. Each stage of the charge pump generally has a diode drop, so this is where the Vgate = 12V typ parameter comes in (3x 5V - 3x Vdiode = ~12V).
So the question is, what is the dropout voltage of the internal regulator. If Vin = 5.5V, will the internal regulator output 5V? The answer is probably no.
About a year ago, I provided you with a waveform on this E2E thread (last page):
e2e.ti.com/.../1290668
With 5.5V Vin, it had about 10V Vgs versus 12V typical at higher Vin. This means the internal regulator is outputting less than 5V.
So we will first check if this is tested in our final test program. If it is not, we can run units in our lab by increasing Vin in increments (5V, 5.1V, 5.2V, 5.3V, etc.) and plot a Vgate vs Vin curve. This would only be one unit, but would give us an idea of how linear the internal regulator performs.
Overall, in order for there to be minimal Vgs (less than 5V at 5.5V Vin), the internal regulator would need to be down to ~2.7V (3x 2.7V - 3x Vd). We see this as very unlikely, as that would mean quite a variance in the regulator dropout voltage. But, running this test should give us initial guidance on how the dropout voltage looks.
Thanks!
Alex