Im using TPS2115A, is the red circle MLCCs effect IN1 and IN2 transition time?
for example, increasing to 1uF, the transition time will increase, please help to cleafy that.
if so, why?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Im using TPS2115A, is the red circle MLCCs effect IN1 and IN2 transition time?
for example, increasing to 1uF, the transition time will increase, please help to cleafy that.
if so, why?
Hi Logan,
This part falls under the Power Interface forum. I will go ahead and move this post there.
Thanks,
Alek Kaknevicius
The value of the IN1/IN2 capacitor should not have an effect on transition time. Are you observing an effect?
HI Eric
Customer observed the transition time different between their design and Intel CRB design,
after compared the component, it's all the same between these two design, except IN1/IN2 capacitor are different.
so I doubt IN1/IN2 capacitor will effect transition time.