Hello,
I need to change a existing POE-PSE design and replace the POE controller. I'm probably going to use the TPS23861 for this and we want to use it in the AUTO mode (and only use the I²C for monitoring)
The POE-PD that we are going to attach contains an 28.7kOhm detection resistor instead of the standard 25kOhm.
For the TPS23861 I find that the accepted resistance range is between 19 and 26.5kOhm and the rejected range is less than 15kOhm or more than 33kOhm.
So it is not in the accepted or the rejected range, will the device accept this and power the device in AUTO mode ?
Thanks,
Koen