Hi All,
We have selected TPS23753A IC for 12V/1A POE module Design.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi All,
We have selected TPS23753A IC for 12V/1A POE module Design.
Hi BEN,
We do not have schematic as we have observed this issue in third party module..
The exact issue is, That POE module get started immediate once input voltage connected but output voltage get reduce toward zero on load condition.
After around 10S of time it will provide full load at ratted voltage.
Another thing is,
Is there any minimum load current requirement to keep signature? We are using adapter oring in secondary side(Output side) with POE output voltage and giving preference to adapter power. For that we have generated 11V from POE circuit and adapter voltage is 12VDC. If some one remove the adapter then the system should not restart. It should continue run from POE power.
Dear Darwin,
Thanks for the reply.
Unfortunately that third party board has damaged during test. We have our own design board by mid of may. If found similar issue in that one then we will share.
Another is,.. That application gives description about primary side oring. We need to do oring on secondary side with 12V adapter. During adapter present, device should take power from adapter and if adapter get fail then device should smoothly get take over on POE circuit without reset. So, for that 10mA blider resistor is sufficient to keep signature?
Regards,
Kalpesh
Dear Darwin,
Thanks for the reply.
Unfortunately that third party board has damaged during test. We have our own design board by mid of may. If found similar issue in that one then we will share.
Another is,.. That application gives description about primary side oring. We need to do oring on secondary side with 12V adapter. During adapter present, device should take power from adapter and if adapter get fail then device should smoothly get take over on POE circuit without reset. So, for that 10mA blider resistor is sufficient to keep signature?
Hi,
Thank You.
There is confusion of 10mA minimum current. We have considered 10mA current on POE Output(12V) but it shows for input.
In our application, We need to make option3 with adapter priority and clause 3.6 for "Keeping the PSE Powered With Options 2 and 3".
For 10mA minimum load it would generate around 0.6W power continuously(Consider 42 to 58V input). Is there any other option to hold Signature without dissipation this power?
If we consider case of low output voltage with only POE(No adapter) like 3.3V with low power requirement design. For 10mA minimum primary current the input power would be 0.010A x 58V = 0.580W. With considering the 75% efficiency the output min load would be 0.580 * 0.75% = 0.435W and minimum output load would be 0.435W / 3.3V = 130mA.
So, If in some condition like sleep mode this load current may be less then 130mA. Will Device get reboot during this scenario?? Blider resistor to keep minimum load is the only solution to prevent re-booting??