Hello,
If the -600V of minus surge is occured at VIN of LM74610-Q1, the voltage within absolute maximum input ?
Since the LM74610-Q1 absolute maximum voltage reference is not GND and there is the Body Diode of FET between Anode and Cathode pins , can we input -600V surge at Vin ?
There is the TVS on the typical application, should we protect the LM74610-Q1 from minus surge? Or this TVS is used for load of LM74610-Q1?
Best Regards,
Ryuji Asaka