Hi,
I am using tps2384 and have following problem: When PD is connected, voltage read from register is ok, but when I disconnect PD, voltage value remains the same. In the other hand, tps current goes to zero.
If I execute POR (by writing to Common Control Write, Register Select = 0001, value 1= reset all circuits and start a POR timing cycle), voltage is set to 0 (for both ports). When connecting the device again, voltage is up. Is there something that I am missing, should I execute some sort of port reset when PD is disconnected? As I understood, device discovery should be performed itself. Again, I couldn't find way to reset values of just one port, is that possible? (If I disable only one port, voltage remains the same)
Thanks in advance for any help,
M