Problem:
When we put overload, IC turns off and doesn't want to turn on again.
VIn=5 V (from 2x30A 5V ORing). Imax is defined as 33,3 A. If we provide more, MOSFET shut off.
Vgate is 0V (before it was 12V).
Once it did turn on again after disconnecting power for long time, now it does not want to start again at all. I'm not sure if IC is still OK,
but I do not see reason why it would get destroyed (IC or perhaps MOSFET).
Any idea if there is failure in design or what we could check?
1-Vout, 2-power good , 3-timer , 4- gate