Hello,
We wanted more clarity on the voltage level of SHTDWN pin of UCC3915DP.
Datasheet mentions the Shutdown threshold as 1.1V to 1.9V, does it mean device will be in shutdown mode (Load turned off) when voltage on SHTDWN pin is with in 1.9V ?
When tested on two UCC3915DP IC's, load was turning ON when voltage on SHTDWN pin is 1.6V. So we wanted to know if the limits of 1.1V to 1.9V provided on the datasheet is for Turn ON or Turn OFF of load. Please refer attachment for schematic and waveforms.
Thank you