The TPS23754 seems ideal for our new design. However, the MIN operating temp of the TPS23754 is -40C, and our system specification is to START/Turn On, not necessarily operate, at -46C. Our expectation is that power can be applied, the normal internal operating circuitry will generate enough heat increase the case temperature to the -40C MIN, then we can actually start and use the TPS23754.
Is this a reasonable assumption? Can we calculate the quiescent power of the device, verify it will, after some time, increase to -40C?
~Leonard