Hi team,
Does TI have 5V current limit switch which Response time to short circuit (tIOS) is less than 1usec?
If [less than 1usec] is impossible, the customer wants to know the part which tIOS is less than typ 3.5usec which is of TPS2556, TPS25200, the customer is using now.
Condition :
* Response time to short circuit (tIOS) : < Typ 1usec ( or < 3.5usec )
* Current limit threshold : Min2A, Max2.5A
* Power switch ON resistance : Max 50mΩ ( Tj : -40C~125C )
Best regards,
Naokazu Kinjoh